Hi and welcome to the documentation for depthai-ros! Here you can find ROS related code for OAK cameras from Luxonis. Don't have one? You can get them here!Main features:
You can use the cameras as classic RGBD sensors for your 3D vision needs.
You can also load Neural Networks and get the inference results straight from camera!
You can develop your ROS applications in following ways:
Use classes provided in depthai_bridge to construct your own driver (see stereo_inertial_node example on how to do that)
Use depthai_ros_driver package (currently available on ROS2 Humble and ROS Noetic) to get default experience (see details below on how)
Supported ROS versions:
Noetic
Humble
Iron
Install from ros binaries
Install depthai-ros. (Available for Noetic, Humble and Iron) sudo apt install ros-<distro>-depthai-ros
Install from source
For installing from source, please refer to this guide.
DepthAI filters
depthai_filters contains small composable node examples that show how to work with data from multiple topics. Available filters:
Detection2DOverlay - subscribes to /nn/detections and rgb/preview/image_raw topics. To see it in action, run ros2 launch depthai_filters example_det2d_overla.launch.py. Note here - If you see that detections misalign in the overlay, adjust rgb.i_preview_size parameter.
SegmentationOverlay, overlays semantic segmentation from /nn/image_raw on top of image from rgb/preview/image_raw, to see it in action, run ros2 launch depthai_filters example_seg_overlay.launch.py
WLS filter - stereo depth filter that smooths out overall depth image based on disparity data. It subscribes to stereo/image_raw and left/image raw topics. Parameters needed to enable it - left.i_publish_topic, stereo.i_output_disparity an example can be seen by running ros2 launch depthai_filters example_wls_filter.launch.py
SpatialBB - publishes bounding boxes as 3D line Markers based on spatial detections coming from driver node
FeatureTrackerOverlay - publishes Tracked Features overlay based on features and images coming from the driver
Features3D - uses depth image to republish features as 3D pointcloud
Custom converters
Users can write Custom converters and plug them in for bridge Publisher. If there a standard Message or usecase for which we have not provided a ros msg or converter feel free to create a issue or reach out to us on our discord community. We would be happy to add more.