Install from source
Install dependencies
The following script will install depthai-core and update usb rules and install depthai devicesCommand Line
1sudo wget -qO- https://raw.githubusercontent.com/luxonis/depthai-ros/main/install_dependencies.sh | sudo bash
sudo apt install libopencv-dev
if you don't have rosdep installed and not initialized please execute the following steps:sudo apt install python3-rosdep
sudo rosdep init
rosdep update
Setting up procedure
The following setup procedure assumes you have cmake version >= 3.10.2 and OpenCV version >= 4.0.0. We selecteddai_ws
as the name for a new folder, as it will be our depthai ros workspace.mkdir -p dai_ws/src
cd dai_ws/src
git clone --branch <ros-distro> https://github.com/luxonis/depthai-ros.git
cd ..
rosdep install --from-paths src --ignore-src -r -y
source /opt/ros/<ros-distro>/setup.bash
catkin_make_isolated
(For ROS1)MAKEFLAGS="-j1 -l1" colcon build
(for ROS2)source devel/setup.bash
(For ROS1) &source install/setup.bash
(for ROS2)
build.sh
command from your workspace (it just wraps colcon commands): ./src/depthai-ros/build.sh
Docker
You can additionally build and run docker images on your local machine. To do that, add USB rules as in above step.Running prebuilt images
Each tagged version has it's own prebuilt docker image. To download and run it:Command Line
1xhost +local:docker
Command Line
1docker run -it -v /dev/:/dev/ --privileged -e DISPLAY -v /tmp/.X11-unix:/tmp/.X11-unix luxonis/depthai-ros:noetic-latest [CMD]
- bash (it will allow you to browse files and make modifications to the code and rebuild it)
- zsh (other shell that is installed that has some advantages over bash)
- roslaunch depthai_ros_driver camera.launch (this is just an example, any launch file will work here) A side note here, launch files in depthai_ros_driver have some default parameters set by .yaml files inside the driver. You can either edit them inside the container itself, or you can make a .yaml file on your host (let's say
/home/YOUR_USERNAME_HERE/params/example_config.yaml
) and pass it as an argument to the executable, as follows:
Command Line
1docker run -it -v /dev/:/dev/ -v /home/YOUR_USERNAME_HERE/params:/params --network host --privileged -e DISPLAY -v /tmp/.X11-unix:/tmp/.X11-unix luxonis/depthai-ros:noetic-latest roslaunch depthai_ros_driver camera.launch params_file:=/params/example_config.yaml
- Install it by running the container in bash/zsh mode
- Modify the Dockerfile so that it's installed during building - you'll have to rebuild the container after that.
- Run base camera node in our container and RTABMap separately on host/ in a separate container (see the launch file on what parameters/topic names need to be changed when running separately).
Building
Clone the repository and inside it run (it matters on which branch you are on):Command Line
1docker build --build-arg USE_RVIZ=1 -t depthai-ros .
BUILD_SEQUENTIAL=1
to build packages one at a time, it should take longer, but use less RAM.RUN_RVIZ
arg means rviz will be installed inside docker. If you want to run it you need to also execute following command (you'll have to do it again after restarting your PC):Command Line
1xhost +local:docker
Command Line
1docker run -it -v /dev/:/dev/ --privileged -e DISPLAY -v /tmp/.X11-unix:/tmp/.X11-unix depthai-ros
Command Line
1docker run -it -v /dev/:/dev/ --privileged -e DISPLAY -v /tmp/.X11-unix:/tmp/.X11-unix depthai-ros roslaunch depthai_examples stereo_inertial_node.launch.py
Running docker image on ROS1
Command Line
1docker run -it -v /dev/:/dev/ --privileged -e DISPLAY -v /tmp/.X11-unix:/tmp/.X11-unix depthai_ros roslaunch depthai_examples stereo_inertial_node.launch
stereo_inertial_node
launch file (you can try different commands).Running docker image on ROS2
Command Line
1docker run -it -v /dev/:/dev/ --privileged -e DISPLAY -v /tmp/.X11-unix:/tmp/.X11-unix depthai_ros ros2 launch depthai_examples stereo_inertial_node.launch.py