Firmware
RAE is powered by the Luxonis OS which is our customized Linux distribution.Manual installation
Connect to your RAE using SSH and execute the following command.Command Line
1mender --install <FIRMARE_URL> && reboot
Command Line
1mender --install https://luxonisos.fra1.digitaloceanspaces.com/build/1.14-rae+6263cb8c60f2cbfc80cc523f2b37581eb38139aa/luxonisos-1.14-rae.dm-verity.mender && reboot
Releases
1.14
DownloadText
1URL:
2https://luxonisos.fra1.digitaloceanspaces.com/build/1.14-rae+6263cb8c60f2cbfc80cc523f2b37581eb38139aa/luxonisos-1.14-rae.dm-verity.mender
3
4SHA256:
57580455e0209072b564ef99375a6db5a19c2f4730baa82fd6b8efb181de21949
1.12
DownloadText
1URL:
2https://luxonisos.fra1.digitaloceanspaces.com/release/1.12/luxonisos-1.12.dm-verity.mender
3
4SHA256:
58d913c09286aec7ae5a401fbb518e0afaf2d8cf0adea615390a95d51d43c44da