Platform

ON THIS PAGE

  • IP rating
  • IP67 rated PoE enclosures

IP rating

IP code tells you whether a device is dustproof and/or waterproof. Only our OAK PoE devices have an IP rating, current version of USB devices do not have an IP rating.

IP67 rated PoE enclosures

Series 1 PoE devices (OAK-D PoE and OAK-1 PoE), OAK-D SR PoE, and OAK Thermal are shipped with an IP67 rated enclosure. IP67 means that the device is protected from total dust ingress and that it's protected from water immersion between 15 centimeters and 1 meter in depth.OAK-D S2 PoE (and all its variants, so -W, -Pro, and -Pro-W) currently have IP65 rated enclosure, and we are working on getting IP67 rating for them.PoE enclosures have gaskets which makes them waterproof/dustproof:Here's our testing of the enclosures. The height of this drum, which was filled with water, is 1 meter and we were testing these two enclosures over an extended period of time.